Industry archive: Power OEMs
2009-02-09 - Circuit-breakers in medium voltage (MV) installations cannot provide any protection against exceptionally high peak short-circuit currents, as they are too slow.
2008-10-29 - To facilitate commissioning, Omicron has made a test template with ABB for REF615, which is a new dedicated feeder protection relay perfectly aligned for the protection, measurement and supervision of utility substations and industrial power systems. Omicron is also working on a test template for transformer protection terminal RET54_.
2008-10-20 - The new ABB FT individual current circuit test plug with open current transformer protection provides a safe, simple, fast, and reliable method to isolate and service installed equipment.
2008-07-17 - Meet the need of domestic power industry customers for high-reliable products
2007-03-26 - This year’s Transmission and Distribution Europe conference was held in Prague, where the conference attendants gathered in March to listen to current topics on energy distribution. The conference participants were mainly senior management people from power utilities. The session topics covered power quality, asset management, information management, security of supply, etc.
2006-10-04 - Milan, 27-28 September Almost exactly half year after the Software User Meeting in Detroit, USA, the first European forum took place at ABB Italy, Milan. About 70 software users from 13 different countries were gathered in Milan during two days focused on software.
2006-09-15 - VisiVolt™ is a novel indicator of voltage presence offered by ABB which can be mounted directly on bare and insulated current bars and conductors of a medium voltage (MV) system. The indicator can be installed both indoors and outdoors, which is a unique feature among indicators of that type. The presence of AC voltage is indicated by appearance of a large and clear lightning arrow sign on the display of the indicator.
2006-08-31 - Curiosity is what drives many visitors to the display of ABB's innovation for switchgear communications at this week's power technologies show in Paris. The waveguide, as it is known, may just look like a silvery metal tube but the simplicity is the key to its advantages.
2006-07-31 - Swiss lab recognized as test facility for global IEC 61850 standard
2006-06-27 - [No lead text]