Archive
2008-09-09 - The ACS 6000, one of the world's most advanced medium voltage variable speed drives, is being used to overcome several technical challenges facing a new, 5 meter wide steel plate mill at Zhangjiagang Hongchang Plate Co., Ltd., one of China’s leading steel manufacturers located in Jiangsu province near Shanghai.
2007-04-11 - BNG Steel Company has ordered a Stressometer 7.0 FSA flatness measurement and control system for the rolling mill in Korea. BNG Steel, with head quarters location in Changwon, is the leading cold-rolled stainless steel producer in Korea with the longest history and the largest capacity of 290,000 tonnes per year. Established in 1966 as Korea's first specialty steel producer, BNG dominated the market with a 25% market share in 2006.
2007-01-09 - At Asian Metallurgy 2007, being held in Mumbai, India on March 1-3, ABB will present the latest product developments in Hall 2B, Booth B 48.
2006-09-15 - At Aluminium 2006, being held in Essen on September 20 – 22, ABB will present the latest product developments in Hall 1, Booth G70.